When you create a new Metric View or open an existing Metric View, the Result section displays the result for the Metric View. This section offers two views of the Metric View, presented on two different tabs: Graph and Table.
By default, the result appears in graph format. The Graph View in the Result section provides a visual representation of the Metric View. You can modify the default graph settings by using button available on the Metric View.
For example, the following graph shows the Event Counts and Average Work Cost based on the criticality of the equipment.
You can change the Graph View to Table View by selecting in the Result section that is displayed on the Graph View. The Table View displays the same information that is displayed on the Graph View, but in a grid format.
Each row in the table corresponds to a value that appears along the x-axis of the graph. The columns in the table represent the values that are plotted on the y-axis of the graph. Using the Table View, you can easily view, the actual values that have been plotted on the graph.
For example, the following table shows the Event Counts and Average Work Cost based on the criticality of the equipment. These same values are represented graphically in the preceding image.
Copyright © 1993-2015 Meridium, Inc. All rights reserved.