Modify the Graph Settings

The graph on the Results workspace provides a visual representation of the Metric View. You can edit the various elements of the graph, such as, the graph type, title, legend placement and so on.

Note: You can edit the graph settings only if you have the Update privilege on a Metric View.

Steps

  1. Access the Metric View page.
  2. In the upper-right corner of the page, select .

    The left pane appears, displaying the dimensions that you have set for the Metric View.

  3. In the upper-right corner of the Results workspace, select .

    The Edit graph settings window appears.

  4. As needed, edit the graph settings.

  5. Select OK.

The Edit graph setting window closes, and the Result section of the workspace displays the modified graph.

Copyright © 1993-2015 Meridium, Inc. All rights reserved.