When you create a Production Event record, on the datasheet, you can select in the Production Event Code cell to select the Production Event Code record that most accurately represents the type of event that the Production Event record represents. Likewise, when you create a Production Event Template record, you can select in the Production Event Code cell to select the Production Event Code record that most accurately represents the type of events that will be created automatically from that Production Event Template record.
Copyright © 1993-2015 Meridium, Inc. All rights reserved.