This topic includes an example of a sequential time-based plan. The data used in this example is listed in tables. In the tables, we list only the fields that contain a value. The information in tables is provided for your reference.
Note: The information contained in these topics assumes that you are the user who will be performing the associated step in creating a Production Plan and that all PLA administrative tasks have been completed.
The example assumes that the PLA Administrator has added the following three Production Profiles to the Production Unit for which you want to create a sequential Time-based Production Plan:
Field | Value |
---|---|
Product 1 | |
Product | Low-Sulfur Diesel |
Product UOM | Units |
Production Rate UOM | Day |
Standard Batch Size | 6,000 |
Standard Batch Cycle Time | 1 |
Max Sustained Capacity Rate | 6,000 |
Product 2 | |
Product | Jet Fuel |
Product UOM | Units |
Production Rate UOM | Day |
Standard Batch Size | 7,500 |
Standard Batch Cycle Time | 1 |
Max Sustained Capacity Rate | 7,500 |
Product3 | |
Product | LPG |
Product UOM | Units |
Production Rate UOM | Day |
Standard Batch Size | 10,000 |
Standard Batch Cycle Time | 1 |
Maximum Sustained Capacity Rate | 10,000 |
The example of a sequential time-based plan assumes that your production plan meets the following criteria:
Criteria | Data Used in This Example |
---|---|
How Much |
Three Products:
|
When |
|
During Which Hours |
Monday through Friday, 24 hours per day, two shifts:
|
How Often You Enter Data | Per Day |
Production Model | Sequential |
Copyright © 1993-2015 Meridium, Inc. All rights reserved.