There is one URL route associated with Production Loss Analysis: failure-elimination/pla. The following table describes the various paths that build on the route, and the values that you can specify for each element in the path.
Element
Description
Accepted Value(s)
Notes
failure-elimination/pla/dashboard/0: Displays the PLA Overview page.
failure-elimination/pla/<EntityKey>/<WorkspaceName>/0: Displays a new or existing Production Data in the Production Data workspace.
Production Data
[ENTY_KEY]Specifies the Production Data that you want to open.
Any numeric Entity Key that corresponds to an existing Production Data.
Opens the specified Production Data in the Production Data workspace.
This value is required to open an existing Production Data from a URL.
0
Opens a new Production Data in the Details workspace.
<WorkspaceName>
Specifies the workspace in which you want to open the Production Data.
data
The specified Production Data will appear in the Production Data workspace.
Production Plans
failure-elimination/pla/<EntityKey>/<WorkspaceName>: Displays an existing Production Plan in the Plan Details workspace.
<WorkspaceName>
Specifies the workspace in which you want to open the Production Plan.
plan
The specified Production Plan will appear in the Plan Details workspace.
Production Events
failure-elimination/pla/0/<WorkspaceName>/<EntityKey>: Displays a new or existing Production Event datasheet in the Production Events workspace.
<WorkspaceName>
Specifies the workspace in which you want to open the Production Event.
eventdatasheet
The specified Production Event datasheet will appear in the Production Events workspace.
Production Analyses
reliability/production/<EntityKey>/<WorkspaceName>: Displays an existing Production Analysis in the Production Analysis workspace of Reliability Analytics.
<WorkspaceName>
Specifies the workspace in which you want to open the Production Analysis.
overview
The specified Production Analysis will appear in the Production Analysis workspace of Reliability Analytics.