Values Mapped from Production Loss Analysis (PLA) to a Production Analysis

When you create a Production Analysis from Production Profile and Production Data records, several fields in the Production Analysis are populated automatically, as shown in the following table.

IMPORTANT: You can create a Production Analysis from PLA only if the license for Reliability Analytics is active

Note: The All Production Data query determines which values from records in the PLA module are mapped to the Production Data field in Production Analysis records. If you want to map values from custom fields to the Production Data field, you will need to modify the All Production Data query

Production Analysis Field Default Value
Analysis ID

A value that is constructed using the following format:

<Production Profile ID> ~ <Start Date> ~ <End Date>

Where:

  • <Production Profile ID> is the ID of the Production Profile that you selected in the Production Analysis Builder.
  • <Start Time> is the start time that you selected in the Production Analysis Builder.
  • <End Time> is the end time that you selected in the Production Analysis Builder.
Start Time The start time that you selected in the Production Analysis Builder.
End Time The end time that you selected in the Production Analysis Builder.
Unit of Measure The value in the Product UOM field in the Production Profile that you selected in the Production Analysis Builder.
Margin Value The value in the Default Margin field in the Production Profile that you selected in the Production Analysis Builder.
Analysis Type The value Production Analysis.
Ignored Points The value 0.
Min Production The value 0.0001.
Production Data

Contains code representing a combination of values that make up the Production Data that is displayed on the Production Analysis plot. This combination of values is mapped from the following fields in PLA:

Production Data records:

  • Actual
  • Period
  • Short Range Plan

Production Loss records:

  • OEE Code
  • Event Code
  • Impact Code
Total Points

The number of Production Data records that meet the following criteria:

  • They are associated with the Production Profile that you selected in the Production Analysis Builder.

    -and-

  • The date in their Period field is on or after the Start Date and on or before the End Date that you selected in the Production Analysis Builder.

Copyright © 1993-2015 Meridium, Inc. All rights reserved.