The following table provides a list and description of the RCM folders that exist by default in the Catalog.
Folder |
Behavior and Usage |
---|---|
\\Public\Meridium\Modules\RCM |
Used to store generic reports related to RCM Analyses. |
\\Public\Meridium\Modules\RCM\Analysis |
Used to store reports related to the RCM Analysis node, which is the root-level node in an RCM Analysis. Several baseline reports are provided in this folder. |
\\Public\Meridium\Modules\RCM\Effect |
Used to store reports related to the RCM FMEA Failure Effect records in an RCM Analysis. |
\\Public\Meridium\Modules\RCM\Equipment List |
Used to store reports related to the RCM FMEA Asset records in an RCM Analysis. |
\\Public\Meridium\Modules\RCM\Failure |
Used to store reports related to the RCM Functional Failure records in an RCM Analysis. |
\\Public\Meridium\Modules\RCM\Function |
Used to store reports related to the RCM Function records in an RCM Analysis. |
\\Public\Meridium\Modules\RCM\Mode |
Used to store reports related to the RCM FMEA Failure Mode records in an RCM Analysis. |
\\Public\Meridium\Modules\RCM\Recommendation |
Used to store reports related to the RCM FMEA Recommendation records in an RCM Analysis. |
\\Public\Meridium\Modules\RCM\SSRS |
Used to store reports that were used in a previous release. This Catalog folder and its contents are not used by the Meridium APM product. |
By default, the baseline RCM product contains a set of pre-configured reports for use with RCM. If desired, you can customize these reports or use them as the basis for creating your own reports. The following table contains a list and description of the baseline RCM reports that are delivered with the baseline RCM product. Note that the Stored In column contains an abbreviated Catalog path, where each of the folders is a subfolder within the Catalog folder \\Public\Meridium\Modules.
In this table, the values listed in the Report column refer to the report names. The baseline captions are the same as the names.
Note that the Catalog folder \\Baseline\Meridium\Modules contains subfolders that match the folders listed in the table. These folders contain copies of the reports that are delivered as baseline RCM content. The items in the \\Baseline folder cannot be modified and serve as a historical record of the items that were delivered with the baseline product. The Meridium APM system reads from the subfolders in the \\Public folder, so the reports in the Baseline folder are not actually used. The \\Baseline folder will be updated with any changes made to the baseline content in future releases.
Report |
Stored In |
Behavior and Usage |
---|---|---|
RCM Analysis Description |
RCM\Analysis |
Provides an overview of the analysis, including the analysis name, analysis description, and a list of the team members and equipment and locations associated with the analysis. This report contains three sections of information:
|
RCM AnalysisTeamSubReport |
RCM |
Used by the report RCM Analysis Description to insert a list of team members involved in the analysis. Note that although this report is stored in the folder \\Public\Meridium\Modules\RCM, the Meridium APM system is hard coded not to display this report on the RCM Reports page. |
RCM FailureModeEffectsAnalysis |
RCM\Analysis |
Provides details of the functions, functional failures, failure modes, and failure effects associated with a given RCM Analysis. |
RCM Recommendations |
RCM\Analysis |
Provides details about each recommendation for all the failure modes in the analysis. Additional, related information such as Consequence and calculated Ranking are also included in the report to provide context for reviewing recommendations. |
Copyright © 1993-2015 Meridium, Inc. All rights reserved.