Create a Functional Failure

Steps

  1. Access the RCM Module Overview page.

  2. Select the analysis for which you want to create a Functional Failure.

    In a new tab, the Analysis Details (Analysis Details) workspace for the selected analysis appears, displaying the Analysis Overview (Analysis Overview) section.

  3. In the left pane select a function.

    The workspace for the selected function appears.

  4. In the left pane, select , and then select Add Functional Failure (Add Functional Failure).

    The workspace for the new Functional Failure appears.

  5. As needed, enter values in the available fields.
  6. Select .

    The Functional Failure is saved.

  7. To return to the analysis, in the left pane, select Analysis Details (Analysis Details).

Copyright © 1993-2015 Meridium, Inc. All rights reserved.