In the upper-right corner of the page, select , and then select Create New Template
The Template Builder
Select Next
The Select Template Type
Select the Template Type you want to use, and then select Next
The Define Root Node
As needed, enter values in the available fields, and then select Next
The Define Template
As needed, enter values in the available fields, and then select Finish
The new Template is added.
Copyright © 1993-2015 Meridium, Inc. All rights reserved.