Access the RA Overview Page for an Asset Hierarchy Level

This topic describes how to view information to improve reliability for an Asset Hierarchy Level. You can also access production information for all the Asset Hierarchy Levels in your organization.

You can perform various tasks on this page based on the membership in various Security Groups.

Steps

  1. In the upper-left corner of the top navigation bar, select .

    The Asset Hierarchy appears.

  2. In the left pane, navigate to the Hierarchy Level for which you want to view the RA Overview page.

  3. In the workspace, select the Performance tab.

    A list of types of performance-related analyses performed on the selected Asset Hierarchy Level appears.

  4. Locate the row that contains a hyperlink that specifies the number of analyses that have been conducted on the selected Asset Hierarchy Level.

    The hyperlink specifies the following:

  5. Select the hyperlink.

    The RA Overview page appears.

    The list of analyses that appear on the following tabs are not associated with specific Hierarchy Level and are, therefore, not filtered based on the selected Asset Hierarchy Level:

    The information that appears on the following tabs and graphs are filtered based on the selected Asset Hierarchy Level:

    RA Overview

    While viewing any of the charts, you can select to customize the appearance of the chart by using standard graph features.

    By default, the hierarchy level is set to Home. You can filter the hierarchy level by selecting in the upper-left corner of the page.

    The Reliability Analytics information on this page is related to an Asset and children of the Asset. If you also want to view Reliability Analytics information that is not related to an Asset, in the Include analyses without any assets box, select Yes.

    You can customize the time period for the information that appears on the tabs or charts. To do so, in the upper-left corner of the RA Overview page, select , and then, in the Period box, enter the desired value of time period.

Copyright © 1993-2015 Meridium, Inc. All rights reserved.