Collect Data for Probability Distribution Analysis

To create a Probability Distribution Analysis, you must select the field that contains the value that you want to analyze.

The following table shows the typical data needed to build and analyze Probability Distribution Analyses.

Data Required Data Type Description Behavior and Usage

Value

Numeric

Select the field that contains the value you want to analyze.

This is a required field.

Censored

Logical

As needed, select the field to provide censoring information. Select the field from the data source that contains a value that indicates censored values.

This field is optional.

Random Variable

Character

If the data source is a query, the name of the random variable and the units of measure will be pre-populated based on the selection you made in the Value field on the previous screen. If you selected a different data source, type the name of the random variable in the Random Variable field and the units of measure for the random variable in the Units field.

This field is optional.

 

Units

Character

Select the units of measure for the random variable.

This field is optional.

Copyright © 1993-2015 Meridium, Inc. All rights reserved.