Define a Process Reliability Line

Steps

  1. Access the Production Analysis for which you want to define a Reliability Line.
  2. In the left pane, select the Production Data tab.

    The Production Data workspace appears.

    Production Data

  3. In the upper-right corner of the workspace, select Production Lines.
  4. In the list, select Reliability Line.
  5. In the Production Data plot, select the point at which datapoints begin to trend away from the Demonstrated Line.

    A dotted line appears and is labeled Process Reliability: <Percentage> , where <Percentage> indicates the reliability of the process.

    The following image shows an example of a Process Reliability line showing that reliability of the process is 56.65%:

    Process Reliability Line

Copyright © 1993-2015 Meridium, Inc. All rights reserved.