Modify the Data in a Reliability Distribution Analysis

Steps

  1. Access a Reliability Distribution Analysis for which you want to modify the data.
  2. In the left pane, select the Probability Plot tab.

    The Probability Plot appears in the workspace.

    Probability Plot

    Note: You can also modify the data for a plot via the Failure Rate Plot, PDF Plot, CDF Plot, PM optimization, and Failure Probability.

  3. In the upper-right corner of the workspace, select Analysis Data, and then select Edit Failure Data.

    The Reliability Distribution Data window appears, displaying the data associated with the selected Reliability Distribution Analysis.

    Reliability Distribution Data

  4. As needed, modify the data in Failures and Assets tab.
  5. Select OK.

    The analysis is updated.

Results

Copyright © 1993-2015 Meridium, Inc. All rights reserved.