Modify the Confidence Level for a Reliability Growth Analysis

Steps

  1. Access the Reliability Growth Analysis for which you want to modify the confidence level.
  2. In the left pane, select the Cumulative <Measurement> Plot tab.

    The Cumulative <Measurement> Plot appears in the workspace.

    Cumulative Measurement

    Note: You can also change the confidence level via the Mean Time Between <Measurement> Plot, and <Measurement> Rate Plot tabs.

  3. In the upper-right corner of the workspace, select Growth Options, and then select Confidence Level.

    The Select Confidence Level window appears.

    Confidence Level

    Note: If the Confidence Level box is disabled, select the Use Confidence check box to activate the confidence level and enable the Confidence Level box.

  4. In the Confidence Level box, select a value from the drop-down to represent the desired Confidence Level.

  5. Select OK.

    The Meridium Enterprise APM system displays the confidence intervals for the analysis based on the percentage you selected in the Confidence Level box.

Copyright © 1993-2015 Meridium, Inc. All rights reserved.