Rename a Reliability Growth Analysis

Steps

  1. Access a Reliability Growth Analysis whose name you want to change.
  2. In the left pane, select the Cumulative <Measurement> Plot tab.

    The Cumulative <Measurement> Plot appears in the workspace.

    Cumulative Measurement

    Note: You can also change the name of the analysis via the Mean Time Between <Measurement> Plot, and <Measurement> Rate Plot tabs.

  3. In the upper-right corner of the workspace, select Analysis Task, and then select Rename.

    The SET ANALYSIS NAME window appears.

    Analysis Name

  1. In the Analysis Name box, enter a new name for the analysis.
  2. In the Analysis Description box, enter a new description for the analysis.
  3. Select OK.

    The analysis name is updated in any appropriate sections on the summary page and in the site map to reflect the change. In addition, the Analysis Description field in any appropriate sections will reflect any changes.

Copyright © 1993-2015 Meridium, Inc. All rights reserved.