Access the RCA Overview Page for an Asset Hierarchy Level

This topic describes how to view the Root Cause Analysis information associated with an Asset Hierarchy Level and its children. You can also access Root Cause Analysis information for all the Asset Hierarchy Levels in your organization.

You can perform various tasks on this page based on the membership in various Security Groups.

Steps

  1. In the upper-left corner of the top navigation bar, select .

    The Asset Hierarchy appears.

  2. In the left pane, navigate to the Hierarchy Level for which you want to view the RCA Overview page.

  3. In the workspace, select the Performance tab.

    A list of types of performance related analyses performed on the selected Asset Hierarchy Level appears.

  4. Select the hyperlink that specifies the number of Root Cause Analyses that have been conducted on the selected Asset Hierarchy Level.

    The RCA Overviewpage appears, displaying the following information for the selected Asset Hierarchy Level:

    RCA Overview

    While viewing any of the above graphs, you can select to customize the appearance of the graph.

    You can filter the hierarchy level by selecting in the upper-left corner of the page.

    By default, the Root Cause Analysis information on the page is related to an Asset and children of the Asset. If you also want to view Root Cause Analysis information that is not related to an Asset, in the Include analyses without any assets? box, select Yes.

Copyright © 1993-2015 Meridium, Inc. All rights reserved.