About Analysis Templates

An Analysis Template is a Root Cause Analysis that is in the Template state.

Analysis Templates are the same as other Root Cause Analyses except that they do not have team members assigned to them and they are always in the Template state (i.e., they never become published). The Analysis Templates can be created either from Root Cause Analyses in either the Published or In progress state and can be used for creating Root Cause Analyses.

Copyright © 1993-2015 Meridium, Inc. All rights reserved.