Rounds Designer Workflow

This workflow provides the basic, high-level steps for using this module. The steps and links in this workflow do not necessarily reference every possible procedure. For more procedures, see the links in the Related Information section.

  1. Create Allowable Values.
  2. Create Measurement Location Templates.
  3. Create ML Template Groups.
  4. Create a Route.
  5. Add Measurement Locations to a Route.
  6. Define a schedule for the Route, Measurement Locations within the Route, or both.
  7. Define the order in which the Measurement Locations should appear on the Route.
  8. Add conditions to the Route.
  9. Add reference documents to the Measurement Locations.

Copyright © 1993-2015 Meridium, Inc. All rights reserved.