The Rounds Data Collection module provides users with the capability to perform route-based, recurring tasks such as operator checks, routine maintenance, lubrication tasks, safety inspections, etc. It provides a user friendly interface for quickly completing the routes and checks when they are due. Generally, data collection will be done using a mobile device such as a tablet computer, as the user completes the required asset checks. Proactive warnings can be set up in the Rounds Designer module to alert the user if the findings indicate a problem with the asset, including advisory notes on what action to take next. Users can create recommendations for action, for example a maintenance follow-up, directly from the mobile device. As data is collected, it is transferred automatically to the Meridium Enterprise APM database, where it is used in various asset performance management workflows, for example monitoring asset health, and tracking completion of preventive maintenance strategies.
Copyright © 1993-2015 Meridium, Inc. All rights reserved.