Add a Nominal Measurement

Steps

  1. Access the TML for which you want to create a nominal measurement.

  2. In the workspace heading, select the TML Details tab.

    The TML datasheet appears, displaying the General Information section.

  3. In the datasheet heading, select the Design General tab, and then, in the Nominal Thickness box, enter a value.

    -or-

    In the datasheet heading, select the Piping tab, and then complete the required fields:

    The Nominal Thickness box is automatically populated with a value based on the values you selected.

  4. Select .

  5. In the workspace heading, select , and then select Nominal Measurements.

    The Nominal Measurements window appears, displaying a list of possible Nominal Measurements.

    Note: Nominal Measurements can only be created for TMLs with no active measurements.

  6. Select the check boxes next to the TMLs for which you want to create measurements.
  7. Select OK.

Results

For each check box you selected, a Thickness Measurement is created and linked to the corresponding TML. The value of the Thickness Measurement is set to the Nominal Thickness value in the TML datasheet.

Copyright © 1993-2015 Meridium, Inc. All rights reserved.