Before an asset can be accessed via the Thickness Monitoring Overview, you must create Corrosion Analysis Settings for that asset.
On the top navigation bar, select .
The Asset Hierarchy appears.
Below the workspace heading, select the Strategy tab, and then, in the Thickness Monitoring row, select TML Groups.
Note: TML Groups will only appear if you have selected an asset. If you have selected a functional location, Assets replaces TML Groups.
The TM page appears, displaying the Corrosion Analysis Settings workspace.
By default, the Inspection Type box is set to UT. Additionally:
Select Create Settings.
Copyright © 1993-2015 Meridium, Inc. All rights reserved.