To Skip Measurements by creating MNT records, the Allow Measurements to be Skipped check box must be selected on the TM Admin Preferences page.
Optionally, you can also select the Allow Consecutive Measurements to be Skipped check box to allow the recording of multiple consecutive MNTs for a single TML without the recording of an actual measurement.
Access Thickness Measurements for the TML to which you want to create an MNT record.
In the upper-right corner of the section, select , and then select Add Skipped Measurement.
The Add Skipped Measurement window appears.
Complete the required fields.
In the Readings box, the default value <Not Taken> will populate and cannot be adjusted by the user.
In theDate box, enter the date for the measurement that you want to skip,
Select Done.
The new MNT record is added to the TML.
Copyright © 1993-2015 Meridium, Inc. All rights reserved.