Receive Data from a Datalogger

Steps

  1. Access Dataloggers for any asset.

    Note: When receiving data from a datalogger, you do not need to select the asset that corresponds to the data. The data will be applied to the appropriate TMLs.

    The TM Dataloggers page appears, displaying the Send To workspace. In the workspace, a list of TMLs appears. By default, all the TMLs are selected.

  2. In the top of the workspace, in the box, select the datalogger to which you want to send the TMLs.

    Note: The datalogger initially displayed in the list will be the last datalogger you used.

  3. Confirm that the datalogger settings are correct.
  4. In the workspace, select the Receive From tab.

    The Receive From workspace appears.

  5. Select Receive.
  6. Select Save.

    The measurements are saved and the Corrosion Analysis is recalculated.

Copyright © 1993-2015 Meridium, Inc. All rights reserved.