System Code Tables Used by TM

The following table lists the System Code Tables used to support various functions throughout Thickness Monitoring.

Table ID Table Description Usage
CITP Corrosion Inspection Type

Populates the Corrosion Inspection Type field in Corrosion Analysis Settings.

You can modify the System Codes in this System Code Table if you want to use custom TML Analysis Types.

CRAM

Corrosion Analysis Methods

Unknown

DPAC Datapoint Access Populates the Access field in TMLs.
DPCN Datapoint Condition Unknown
DPCR Datapoint Corrosion Analysis Methods Populates the Corrosion Rate Options in Corrosion Analysis Settings.
DPIN Datapoint Insulation Unknown
DPTP Datapoint Type Unknown
DSCD Design Code Populates the Design Code list in TMLs.
INST Inspection Status Code Unknown
INSM Inspection Interval Types Unknown
MI ASSET TYPE Asset Type Populates the Asset Type list in Thickness Monitoring Rules Lookup records.
MI RESOURCE ROLE List of user roles Populates the Role list in Resource Role records.
MI STATUS INDICATOR TML Status Indicator Populates the Status Indicator list in TMLs.
PIPFMU Pipe Formula Populates the Formula Classification list in Thickness Monitoring Rules Lookup records.
PVFMU Pressure Vessel Formula Populates the Formula Classification list in Thickness Monitoring Rules Lookup records.
SLCR Straight Line Corrosion Methods Unknown
T MIN CUSTOM EQUATIONS T-Min Calculator Custom Equations Unknown.
STCR Statistical Corrosion Methods Unknown
TNKT Tank Type Populates the Component Type list in Thickness Monitoring Rules Lookup records.
VSTP Vessel Type Populates the Component Type list in Thickness Monitoring Rules Lookup records.

Other standard System Code Tables, such as UOME, MATG, and MATL, are also used in Thickness Monitoring.

Copyright © 1993-2015 Meridium, Inc. All rights reserved.