The Catalog folder \\Public\Meridium\Modules\Thickness Monitoring contains the following folders with content:
The Catalog folder \\Public\Meridium\Modules\Thickness Monitoring\Graphs contains the following items.
Item Name | Behavior and Usage |
---|---|
Corrosion Rate Dist | This graph appears on the Thickness Monitoring Overview page, and is based on the Corrosion Distribution query. It displays the corrosion rates of assets with calculated Asset Corrosion Analyses, ordered from highest rate of corrosion to lowest. |
Remaining Life Less than 180 Months Graph | This graph appears on the Thickness Monitoring Overview page, and is based on the Remaining Life Less than 180 Months query. It displays the remaining life of assets with calculated Asset Corrosion Analyses, ordered from lowest remaining life to highest. |
The Catalog folder \\Public\Meridium\Modules\Thickness Monitoring\Queries contains the following items.
Item Name | Behavior and Usage |
---|---|
Assets Near or Past Retirement | Used on the Thickness Monitoring Overview workspace to return a list of all assets with Asset Corrosion Analyses that are within 5 years of or past the retirement date. The list is displayed when you select the Assets Near or Past Retirement Date tab. |
Assets with TM Tasks | Used on the Thickness Monitoring Overview workspace to return a list of all assets with Thickness Monitoring Tasks. The list is displayed in the TM Tasks box. |
AvailableTMTasks | Returns all Thickness Monitoring Tasks related to the supplied assets. |
Corrosion Distribution | Used to populate the data in the Corrosion Rate Distribution graph on the Thickness Monitoring Overview workspace. |
Degradation Rates Greater than Expected | Used to populate the list in the Degradation Distribution box on the Thickness Monitoring Overview workspace. |
Excessive Corrosion | Used on the Thickness Monitoring Overview workspace to return all assets with Asset Corrosion Analyses, and a Controlling Corrosion Rate greater than 20 Mils/year. The list is displayed when you select the Excessive Corrosion tab. |
Measurement Input Reference | Returns TMLs and additional reference data used for entering Thickness Measurements in the Measurement Data Entry workspace. |
Measurements Near or Less than T-Min | Used on the Thickness Monitoring Overview workspace to return all assets with measurements that fall within 10 Mils or less of T-Min. |
Remaining Life Less than 180 Months | Used to populate the data in the Remaining Life graph on the Thickness Monitoring Overview workspace. |
Thickness Inspections | Used on the Thickness Monitoring Overview workspace to return all assets with a Next Inspection Date, including past dates. This list is displayed when you select the Thickness Inspections tab. |
TM Assets | Used on the Thickness Monitoring Overview workspace to display a list of all assets with Thickness Monitoring data linked to the selected Functional Location. |
TM Assets Requiring a Calculation | Used on the Thickness Monitoring Overview workspace to display a list of all assets with Asset Corrosion Analyses that must be recalculated. This list is displayed when you select the Assets Requiring a Calculation tab. |
TM Overview Filter Parameters | None. |
TML Groups for an Asset | Returns a list of all TML Groups linked to the selected asset. |
TMLs for an Asset | Returns a list of all TMLs linked to the selected asset or TML Group. |
Copyright © 1993-2015 Meridium, Inc. All rights reserved.