To add a hyperlink to a graph, you must access the query that is used to generate the graph. This topic describes how to add an internal URL or an external URL that you have configured in the query that is used to generate the graph.
Access the graph for which you want to add a hyperlink.
Hint: You can also access a graph from the catalog.
In the upper-right corner of the workspace, select .
The Settings pane appears.
Select the Series tab.
The Series section appears.
In the Hyperlink box, select the hyperlink that you want to add to the axis that you have selected.
The hyperlink is added to the graph.
Copyright © 1993-2015 Meridium, Inc. All rights reserved.