Open topic with navigation
Create a HAVING Clause
Steps
- Access the Design workspace for the query within which you want to create a HAVING clause.
- In the Conditions section, make sure the Show Totals check box is selected.
- In the Total cell of the desired field, in the drop-down list, select any option other than Where.
- Access the Expression Builder window from the Criteria or Or cells, enter the necessary parameters, and then select Done.
Results
Copyright © 1993-2015 Meridium, Inc. All rights reserved.