Create a New Dashboard

Steps

  1. Access the Dashboards page.
  2. In the upper right corner of the Dashboards page, select Create New.

    The Save As window appears.

  3. In the Catalog pane, navigate the hierarchy to determine the type of dashboard that you want to create.
  4. A grid appears in the workspace.

  5. Under the grid, complete the required fields.

  6. Select Save.

    A blank dashboard appears on the Dashboard page, and the dashboard is saved to the Catalog.

Copyright © 1993-2015 Meridium, Inc. All rights reserved.