When you build a prompt that displays a list of System Codes, the prompt will display a list of values pulled from a selected table of system codes. For example, you could build a prompt on the Critical Asset? field that presents the values Yes and No from a system code table in a query that returns pumps.
In the Valid Values list, select Values From a System Code Table, and then select Next.
The Values From a System Code Table section appears.
Select the Allow Multiple Selections check box if you want users to be able to select multiple values by which to filter the query results.
Note: The Allow Multiple Selections check box is enabled only if you select the Values are Exclusive check box.
Select Next.
The Configure Default Prompt Selection section appears.
If you want a particular value to be selected by default, then select the row containing the necessary value, and then select Finish.
Note: You can select multiple default prompt values only if the Prompt Data Type is set to Character, and you selected the Allow Multiple Selections check box in the Values From a System Code Table section.
The prompt appears in the Expression Builder window.
Select Done.
The Expression Builder window closes, and then, in the grid in the Conditions section, <expr> appears in the field on which you created the prompt.
Copyright © 1993-2015 Meridium, Inc. All rights reserved.