A dataset is a fixed set of information that is stored as a Catalog item.
Datasets contain information that can be viewed and modified in a grid. While queries return the most current information in the database, a dataset displays the same information until it is modified manually. For example, you might use a dataset to store information from an external system so that the data can referenced or used to create graphs in Meridium Enterprise APM.
When a dataset is created, a data type is defined for each column to indicate the type of data that can be stored in cells in that column. When you create or modify a dataset, if you attempt to enter data that conflicts with the data type defined for that column, the data will not be retained. The following types of data can be stored in a dataset:
You can create new datasets manually within Meridium Enterprise APM, or by importing a Microsoft Excel file (.xls or .xlsx), an XML file (.xml), or a text file (.txt or .csv).
After you create a dataset, you can access it, modify it, use it to create graphs, and export it as a Microsoft Excel file, an XML file, or a text file.
Related Information
Copyright © 1993-2015 Meridium, Inc. All rights reserved.