When you add a query source to the design canvas, system and inactive fields are not displayed in the field list. You might, however, want to add system or inactive fields to the query. You can make these fields available for use in a query by using the following instructions.
Select the source node for which you want to display system or inactive fields.
The window for the selected source node appears.
In the window, in the Fields section, select . Then, in the drop-down list, select either one or both of the Show System Fields and Show Inactive Fields check boxes.
Depending on your selection, the system and/or inactive fields for the family appear in the Fields section, at the end of the list. System fields are identified by their field IDs, and inactive fields are identified by their field captions appearing within square brackets.
Copyright © 1993-2015 Meridium, Inc. All rights reserved.