Show or Hide Grid Lines

Steps

  1. Access the graph for which you want to show or hide the grid lines.

    Hint: You can also access a graph from the catalog.

  2. In the upper-right corner of the workspace, select .

    The Settings pane appears.

    The Graph section of the Settings pane

  3. Select Axis.

    The Axis section appears.

    The Axis section of the Settings pane

  4. If you want to show the grid lines, select the Grid Lines check box.

    The graph is refreshed to display the grid lines.

  5. If you want to hide the grid lines, clear the Grid Lines check box.

    The graph is refreshed to hide the grid lines.

Copyright © 1993-2015 Meridium, Inc. All rights reserved.