Access the graph for which you want to show or hide labels.
Hint: You can also access a graph from the catalog.
In the upper-right corner of the workspace, select .
The Settings pane appears.
If you want to view the vertical axis labels, in the pane, in the Graph section, select the Show Labels check box.
The graph is refreshed to show the vertical axis labels.
If you want to view the x-axis labels, in the pane, in the Graph section, select the Show X-Axis Labels check box.
The graph is refreshed to show the x-axis labels.
If you want to hide the vertical axis labels or the x-axis labels, clear the Show Labels or Show X-Axis Labels check box, respectively.
The graph is refreshed to hide the labels.
Copyright © 1993-2015 Meridium, Inc. All rights reserved.