Access the graph for which you want to show or hide the scroll bar.
Hint: You can also access a graph from the catalog.
In the upper-right corner of the workspace, select .
The Settings pane appears.
If you want to view the scroll bar, in the pane, in the Graph section, select the Show Scroll Bar check box.
The Maximum amount of points to show box appears.
In the Maximum amount of points to show box, enter the number of points that you want to view per page.
The graph is refreshed to show the specified number of points per page. You can use the scroll bar to view the rest of the pages.
If you do not want the scroll bar, in the pane, in the Graph section, clear the Show Scroll Bar check box.
The graph is refreshed to show all the points on a single page.
Copyright © 1993-2015 Meridium, Inc. All rights reserved.