Access the graph for which you want to specify the number of decimals for the vertical axis values.
Hint: You can also access a graph from the catalog.
In the upper-right corner of the workspace, select .
The Settings pane appears.
Select the Axis tab.
The Axis section appears.
In the Decimals box, select the number of decimals for the vertical axis values.
Note: If the value in the Format field is None, then the vertical axis values do not contain decimals.
The graph is refreshed to plot the vertical axis values with the specified number of decimals.
Copyright © 1993-2015 Meridium, Inc. All rights reserved.