You can add either a parent OEE Code or an OEE Code that is the child of an existing parent.
Steps
In the Choose codebox, select OEE Codes.
The list of OEE Codes appears.
To add a parent OEE Code at the top level of the hierarchy, select
-or-
To add a child OEE Code to an existing parent, select the check box next to the parent, and then select
The Add OEE Code window appears.
Select
The OEE Code is saved.
Copyright © 1993-2015 Meridium, Inc. All rights reserved.