In PLA, the values that are calculated by the Meridium Enterprise APM system will be displayed using the number of decimals defined in the Settings window. You can change the number of decimal places that appear for the Monetary and Quantity fields using the following instructions.
Steps
On the upper-right corner of the page, select Settings.
The Settings window appears.
In the Quantity Precision box, enter the required number of decimal places for all the quantity fields, such as Actual, Losses, Short Range Plan, Unaccounted Loss, MSC. This value must be greater than or equal to 0 (zero) and less than or equal to 9. By default, the value in this field is set to 0.
Select Save.
The precision values are saved.
Copyright © 1993-2015 Meridium, Inc. All rights reserved.