What is Meridium Enterprise APM?

Production facilities often face problems related to recurring equipment failures, including:

Data related to equipment failures and the impact that they have on a facility can be recorded using a data collection tool. Collecting failure data alone, however, cannot prevent the same problems from occurring in the future. What production facilities need is a tool that will analyze the failure data to help decrease the number of equipment failures, which will in turn increase profit margins.

The Meridium Enterprise APM system fulfills this need.

You can use Meridium Enterprise APM tools to analyze and process data that is collected in and transferred from an external system (e.g., SAP). After the data exists in Meridium Enterprise APM, it can be analyzed to determine the state of your equipment and the reliability, trends, potential risks, and probability of failures associated with that equipment. Based on the gathered data and associated analyses, you can map out the impact of projected changes and then make recommendations and suggest strategies for future equipment maintenance.

Copyright © 1993-2016 Meridium, Inc. All rights reserved.