Overview of the AMS Analytics Module

You can use the AMS Analytics module to view and analyze data that exists in an external AMS Analytics data source, which may include any of the following:

Using AMS Analytics, you can transfer data from AMS Analytics data sources into the Meridium Enterprise APM database. When the data is transferred, records in the AMS Analytics data model are created automatically and populated with values from the data source.

All of the AMS Analytics data sources listed above are components of the AMS Suite and store information that is reported about AMS Assets, such as alerts and events, to provide an indication of their overall health. AMS Assets typically represent smart sensors that report events related to either the health of the asset (e.g. equipment or functional location) that the sensor is monitoring or the health of the sensor itself. By incorporating this information into your Meridium Enterprise APM implementation, you can use the tools in AMS Analytics to assess the overall health of sensors and the related assets in your facility.

You can use AMS Analytics to:

Copyright © 1993-2016 Meridium, Inc. All rights reserved.