APM Connect Data Loaders provide users with the ability to import data from external sources into the various Meridium modules. For example, if a user needs to migrate Thickness Monitoring data from a point solution, a data loader could be used to accomplish this data integration.
All of the data loaders share common capabilities and architecture. Each one uses an Excel workbook as the source of data to be loaded into Meridium Enterprise APM, and each contains the intelligence to load the specific data model for which it was intended. The data is imported using Meridium, Inc's web services.
Copyright © 1993-2016 Meridium, Inc. All rights reserved.