Add an Inspection Method

Steps

  1. Access the existing Inspection Methods for the selected asset.
  2. In the Inspection Methods section, in the Category column, select the empty row.
  3. A drop down list appears, displaying possible types of inspections for the new Inspection Method.

  4. In the Category box, select the type of Inspection for the new Inspection Method.

  5. Note: The only field required to add a new inspection method is the Category field. Once you select a Category value, a new row appears in the grid. You can then add additional Inspection Methods.

  6. Select .

    The Inspection Methods are saved.

Copyright © 1993-2016 Meridium, Inc. All rights reserved.