Create an Inspection Task

Steps

  1. Access the Inspection Management Overview page for the Inspection asset to which you want to add an Inspection Task.
  2. On the upper-right corner of the page, select , and then select Create Inspection Task.

    On a new page, an Inspection Task datasheet appears.

  3. As needed, enter values in the available fields, and then select .
  4. Note: The Inspection Task datasheet inherits the required values from the selected Inspection Family. You do not have to enter any values in the Inspection Task datasheet; however, you can modify the datasheet prior to saving.

    The Inspection Task is saved.

Copyright © 1993-2016 Meridium, Inc. All rights reserved.