Work Packs store preparation information about inspection work that needs to be performed for equipment and/or locations. The following table provides an alphabetical list and description of the fields that exist in the Work Pack family. By default, all fields in the Work Pack family appear on the Work Pack datasheet.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
Field | Data Type | Description | Behavior and Usage |
---|---|---|---|
Preparation Details |
Text |
Preparation information about the inspection work associated with the Work Pack |
You can enter any preparation details about the inspections in this field. |
Work Pack ID |
Character |
The Record ID of the Work Pack |
This is a required field. You must enter a value in this field before you can save a Work Pack. |
Work Pack Description |
Character |
A description of the Work Pack |
This is a required field. You must enter a value in this field before you can save a Work Pack. |
Copyright © 1993-2016 Meridium, Inc. All rights reserved.