About Meridium Inner Joins

When you use two related entity families as query sources, Meridium Enterprise APM creates an inner join between the two entity families by default. This inner join causes the query results to include only the records that are linked through the specified relationship.

If two entity families are not related through a relationship family, you can manually create an inner join to connect one or more fields in one family to one or more fields in the other family.

The following table shows the line style that appears in the design canvas to represent Meridium inner joins.

Join Type Line Style
Meridium Inner Join

Copyright © 1993-2016 Meridium, Inc. All rights reserved.