A number/mathematical function is used to manipulate values returned on numeric fields.
The following table provides a list of the number/mathematical functions that you can use in queries. The Oracle Function column contains the function you will need to use if you are using an Oracle schema. The SQL Server Function column contains the function you will need to use if you are using a SQL Server database.
In some cases, a function cannot be expressed on both an Oracle schema and a SQL Server database. In these cases, the Oracle Function or SQL Server Function column contains an empty, shaded cell.
Description | Oracle Function | SQL Server Function |
---|---|---|
Absolute value | ABS | ABS |
Arc cosine | ACOS | ACOS |
Arc sine | ASIN | ASIN |
Arc tangent of n | ATAN | ATAN |
Arc tangent of n and m | ATAN2 | ATAN2 |
Smallest integer>=value | CEIL | CEILING |
Cosine | COS | COS |
Hyperbolic cosine | COSH | COT |
Exponential value | EXP | EXP |
Largest integer<=value | FLOOR | FLOOR |
Natural logarithm | LN | LOG |
Logarithm, any base | LOG(N) | LOG(N) |
Logarithm, base 10 | LOG(10) | LOG10 |
Modulus (remainder) | MOD | USE MODULO(%) OPERATOR |
Power | POWER | POWER |
Random number | RAND | |
Round | ROUND | ROUND |
Sign of number | SIGN | SIGN |
Sine | SIN | SIN |
Hyperbolic sine | SINH | |
Square root | SQRT | SQRT |
Tangent | TAN | TAN |
Hyperbolic tangent | TANH | |
Truncate | TRUNC | |
Largest number in list | GREATEST | |
Smallest number in list | LEAST | |
Convert number if null | NVL | ISNULL |
Copyright © 1993-2016 Meridium, Inc. All rights reserved.