Create a HAVING Clause

Steps

  1. Access the Design workspace for the query within which you want to create a HAVING clause.
  2. In the Conditions section, make sure the Show Totals check box is selected.
  3. In the Total cell of the desired field, in the drop-down list, select any option other than Where.
  4. Access the Expression Builder window from the Criteria or Or cells, enter the necessary parameters, and then select Done.

Results

Copyright © 1993-2016 Meridium, Inc. All rights reserved.