When you create a prompt that presents a list of results from another query, the prompt selection dialog box will display a drop-down list of values retrieved by running that query.
Hint: You can use a prompt with a list of query results to filter a dependent prompt's values.
You can use only a Select query for generating a list of prompt values. Note that:
If the selected query contains more than one column, the list of prompt values will contain a concatenated list of values from the second column and each subsequent column. For example, if the query results look like this table:
Equipment ID | Manufacturer | Description | Status |
---|---|---|---|
123 | Alco | Tank | Active |
456 | Whitlock | Pump | Inactive |
789 | Delta | Pressure Vessel | Active |
...the list of prompt values will look like this:
Note that the values from the first column, Equipment ID, are not displayed as part of the prompt values.
Hint: Select Unique Values Only in the prompt query to keep the prompt list from containing duplicate values.
Steps
In the Valid Values list, select Values From Query, and then select Next.
The Values From a Query section appears.
In the text box, enter SQL code directly. If you completed this task, then proceed to Step 6.
-or-
Select Browse.
The Select a query from the catalog window appears.
Select the Allow Multiple Selections check box if you want users to be able to select multiple values by which to filter the query results.
Note: The Allow Multiple Selections check box is enabled only if you select the Values are Exclusive check box.
Select Next.
The Configure Default Prompt Selection section appears.
If you want a particular value to be selected by default, then select the row containing the necessary value, and then select Finish.
Note: You can select multiple default prompt values only if the Prompt Data Type is set to Character and you selected the Allow Multiple Selections check box in the Values From Query section.
The prompt appears in the Expression Builder window.
Select Done.
The Expression Builder window closes, and then, in the grid in the Conditions section, <expr> appears in the field on which you created the prompt.
Results
Copyright © 1993-2016 Meridium, Inc. All rights reserved.