Export a Query Result Set to a File

Steps

  1. For the Select query for which you want to modify the output mode, access the Design workspace.
  2. In the upper-right corner of the workspace, select , and then select Export to a File.

    The Export to a File window appears.

    Query Export

  3. In the box, provide the file name.

  4. In the drop-down list, select the desired file type, and then select Export.

    The exported file will download via your browser.

  5. Save the file to the desired location.

Copyright © 1993-2016 Meridium, Inc. All rights reserved.