Modify the Output Mode of a Select Query

Steps

  1. For the Select query for which you want to modify the output mode, access the Design workspace.
  2. In the grid in the Conditions section, depending on which mode you want to use, select or clear the Formatted check box as needed.
  3. In the content header, select .

    The query is run in the selected mode, and the results appear.

    Hint: You can save the query to save the selected mode. The next time you run the query, it will use the mode that was selected when it was last saved.

Copyright © 1993-2016 Meridium, Inc. All rights reserved.