About Custom Line

After you have drawn the Demonstrated Line, the Process Reliability Line, and the Nameplate Line, you can optionally draw one or more additional Custom Lines to compare historical or projected production rates to the observed production rate. For example, you might draw a Custom Line:

The following image shows a Custom line drawn using a Beta value of 10 and Eta value of 1:

Custom Line

Copyright © 1993-2016 Meridium, Inc. All rights reserved.